Change Language :

The maritime industry is at a turning point when it comes to reducing its environmental impact and promoting more sustainable practices. The electricity requirements of ocean-going vessels are comparable to those of a small town. Until now, this power has been generated on board by diesel generators, which has led to considerable pollution and noise emissions. A change of mindset has taken place. A key technology that helps drive this transformation is the shore power solution.
The ports are now striving to supply ships with shore power - without local air pollution, without consuming fossil fuels and without causing greenhouse gas emissions.
We are at the forefront of developing innovative systems that enable ships to switch to clean energy sources in port. In this blog, we will highlight the environmental benefits of igus shore power and explain why this technology is so important for the future of our ports.

The use of shore power can significantly reduce greenhouse gas (GHG) emissions and air pollutants such as nitrogen oxides (NOx), sulphur oxides (SOx) and soot particles. Using shore power from renewable energy sources can reduce CO₂ emissions by up to 100%. One of the biggest advantages of shore power is the drastic reduction in harmful emissions. Ships that switch to shore power in port can shut down their diesel generators. This leads to a significant reduction in nitrogen oxides, sulphur oxides, particulate matter and carbon dioxide. These emission reductions are not only good for our planet, but also for the health of people who live and work near ports.

Reducing ship emissions significantly improves air quality in and around port areas. This is particularly important for cities where the port is an integral part of urban life. Cleaner air means fewer respiratory illnesses and a higher quality of life for local residents and port workers. In addition, shore power contributes to a quieter environment as the ship's engines and generators can be switched off. This reduction in noise promotes a stress-free and more pleasant atmosphere.

Shore power is often more efficient than power generation on board ships. When this power comes from renewable sources, efficiency is increased even further, leading to an even greater reduction in the carbon footprint. By using shore power, ships can reduce their consumption of fossil fuels. This not only helps reduce pollution but also lowers operating costs for shipping companies, providing long-term economic benefits.

Shore power systems are an essential component of green port initiatives aimed at minimising the environmental impact of ship traffic. They demonstrate the commitment of port authorities and shipping companies to make the maritime industry more environmentally friendly. The implementation of shore power systems is a clear indication that the maritime industry is ready to invest in sustainable technologies. This not only promotes environmental compatibility but also strengthens the industry's image as responsible and future-oriented.

The igus Mobile Shore Power Outlet (iMSPO) is an innovative solution specially developed to meet the challenges of shore power supply. The iMSPO system offers a flexible and mobile solution for shore power connections along the entire berth. This is particularly useful in ports with varying tides and different ship lengths. This flexibility allows ports to operate more efficiently and sustainably.
For more information about our shore power solutions, please visit our igus shore power website.