chainflex® cables for use in the offshore industry

Unique around the world: chainflex cables with "DNV" approval

New test stand for cables in moving applications guarantees reliability in maritime use

To allow cables to be used for moving applications on ships and offshore applications without the need for time-consuming and cost-intensive special approvals, igus GmbH and the DNV classification company developed a new test procedure. As a result, a total of 387 chainflex cables from igus have now received type approval for permanent movement in e-chains. This makes them the first cables in the world specifically for applications in energy chains to receive this approval.
chainflex cables DNV approval
In order to supply safe and suitable products for these applications, igus GmbH from Cologne worked with the DNV classification company to develop a new testing procedure and to have their chainflex cables certified.
 
Development of new testing procedures necessary 
Classification companies such as DNV typically issue approvals that are in line with international standards. In many cases, particularly concerning the materials, these refer to special specifications with regard to fire behaviour or other requirements.
Over a long certification time of more than three years, with very different areas of investigation, the special knowledge of the two companies led to a cable designation for use in energy chains on ships and in offshore applications for the very first time.

White paper: more automation in the maritime sector

What challenges, what advantages do automation and digitalisation bring to the maritime industry? How can companies meet the strict test criteria to have components certified by competent institutions such as DNV? What opportunities arise for suppliers, plant manufacturers and operators of drilling platforms and ships through the use of certified components such as B. cables?


MUD-resistant according to NEK606

NEK 606 is a Norwegian standard for all cables used in offshore applications. 301 chainflex cables comply with the requirements of the NEK 606 standard.
NEK 606 logo

Control cables

CF77.UL.D - control cable

CF77.UL.D - control cable

CF78.UL - control cable

CF78.UL - control cable

CF2 - control cable

CF2 - control cable

CF9.UL - control cable

CF9.UL

CF10.UL - control cable

CF10.UL

Data cables

CF112 - data cable

CF112 - data cable

CF211.PUR - data cable

CF211.PUR

CF240.PUR - data cable

CF240.PUR

Bus cables

CFBUS.PUR - Bus cable

CFBUS.PUR

CFBUS - bus cable

CFBUS

Fibre-optic cable (FOC) PUR

CFLG.LB. PUR - fibre optic cable

CFLG.LB. PUR

Measuring system cables

CF113.D - measuring system cable

CF113.D - measuring system cable

CF111.D - measuring system cable

CF111.D

Servo cables

CF270.UL.D servo cable

CF270 - servo cable

CF27. D - servo cable

CF27. D - servo cable

Motor cables

CF27.D - motor cable

CF27.D

CF34.UL.D - motor cable

CF34.UL.D

CF35.UL - motor cable

CF35.UL

CF270.UL.D - motor cable

CF270.UL.D

CFPE - motor cable

CFPE

CF310.UL - motor cable

CF310.UL

CF300.UL.D - motor cable

CF300.UL.D

The rolling energy chain for long travels and heavy duty

The roller energy chain has been the tried-and-tested energy supply for long travels for about 20 years. The successful design that characterises all our linear energy chain systems is supplemented by rollers made of stainless steel, which upgrade the energy chain to an energy supply for heavy-duty applications. As the energy chain rolls and does not glide, it runs silently and with low vibration. The wear is significantly lower than with a design without rollers, and the power needed for the movement is also about 57% lower.
The evolution of the rol e-chain®
P4.1 The newest generation of the rol e-chain P4.1 with a smart sensor

e-chains with cables in the test laboratory

chainflex test laboratory

Largest test laboratory for moving cables. 25 years of experience. 3.800m² test area


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH